Hard Fault when reading flash
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 3:17 AM
I am working to generate the CRC for the flash memory, During this I am facing hard fault when the CRC module tries to read from certain flash locations, to debug it I made a small loop which assigns the value of each 4 byte. I found that reading at certain locations results in hardfault.
I tried with different starting address, I found that
when starting address is 0x08000000 hardfault occurred at 0x08000440
when starting address is 0x08001000 hardfault occurred at 0x0800144c
when starting address is 0x08004000 hardfault occurred at 0x080044cc
uint32_t *d1 = 0x08000000;
while(length){
uint32_t temp = *d1;
d1++;
length -= 4;
}
Any Idea of what is causing this issue?
- Labels:
-
CRC
-
STM32H7 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 5:01 AM
> volatile uint32_t temp = *d1;
> The address in d1 is 0x80029d0 at the time of hardfault, another time is 0x800332c...
The causative assembler instruction and the relevant register values would be interesting.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 5:08 AM
Hmm, I've injected those addreses into register sourced by ldr and no issues. :|
Does your dissassembly really uses proper addreses? Still may be compiler difference. I don't have gcc toolchain installed right now.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 5:31 AM
I created a new project and the above code snippet works fine without issues. compared both the snippets the suspicious difference I found is, in the project where I had the hardfult the vector table was moved to sram in system_stm32h7xx.c file(#define VECT_TAB_SRAM), Once I commented it out its working fine. I could not understand how this causes hardfault at random flash address?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 5:36 AM
You've got some interrupt faulting. You haven't shown assembler or registers at faulting point, so hard to debug through the keyhole.​
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
‎2019-12-12 5:39 AM
The vector table has a 2^8 address alignment requirement (if I remember correctly). A word address (32 bit) is not sufficient.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 5:41 AM
Check linker output file - what addressed are used for interrupts routines and are they coherent with the addreses of offsetted vector table. So the crash could be caused by sth like debug exception, not the code itself.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 5:58 AM
I created a new project and the above code snipped worked without any issues, on comparing the old and new ones, I found that old one uses the RAM for vector table enabled by #define VECT_TAB_SRAM in system_stm32h7xx.c file, once I commented out the old one also worked fine. Could not understand how this causes hard fault?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-12-12 6:13 AM
Looks like the change has no effect in moving the vector, the map file shows the following output, irrespective of defining the flag. This could have caused the issue.
0x0000000008000904 0x2 Core/Startup/startup_stm32h743zitx.o
0x0000000008000904 RTC_Alarm_IRQHandler
0x0000000008000904 EXTI2_IRQHandler
0x0000000008000904 TIM8_CC_IRQHandler
0x0000000008000904 HRTIM1_Master_IRQHandler
0x0000000008000904 UART8_IRQHandler
0x0000000008000904 SPI4_IRQHandler
0x0000000008000904 TIM1_CC_IRQHandler
0x0000000008000904 BDMA_Channel6_IRQHandler
........
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-12 9:18 PM
Did you find the cause of this issue? I"m seeing the same thing.. just assigning a pointer to the sector start, and then reading, causes the hard fault... or sometimes it reads 0, but the data flashed is not 0 :
uint32_t *pFlash = (uint32_t*)(0x81e0000);
uint32_t ulData;
ulData = pFlash[0];
Interestingly, if I power off the stm32h7 disco, the read works again, but can get it to fail by, unlock, write data then locking again. Everything returns HAL_OK, yet the very next read of the flash causes the hard fault.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-13 3:48 AM
Is data cache enabled?