2020-02-06 01:32 AM
We need a powerful M7 core running at high speed + GPU support for TouchGFX. It seems that STM32F750 is a perfect match, apart from the fact that it is missing support for on-the-fly decryption (OTFD). As we would like to use external flash memory and encrypt it, we will need OTFD support. I know that the new STM32 models that are launched have it on board. Is there a launch planned for a model similar to F750 but with OTFD support?