cancel
Showing results for 
Search instead for 
Did you mean: 

Fail to build SBSFU example

jvieira88
Associate II

Hi, I'm starting to play with the SBSFU examples provided by ST. I'm trying to build the SBSFU (mcuboot based) example for the STM32L5 which can be found in the STM32SecuWS provided here . 

I'm stuck trying to build the TFM_SBSFU_boot (partial console output):

arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/low_level_com.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/low_level_com.d" -MT"Application/User/low_level_com.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/low_level_com.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/low_level_device.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/low_level_device.d" -MT"Application/User/low_level_device.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/low_level_device.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/low_level_flash.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/low_level_flash.d" -MT"Application/User/low_level_flash.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/low_level_flash.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/low_level_ospi_device.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/low_level_ospi_device.d" -MT"Application/User/low_level_ospi_device.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/low_level_ospi_device.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/low_level_ospi_flash.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/low_level_ospi_flash.d" -MT"Application/User/low_level_ospi_flash.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/low_level_ospi_flash.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/low_level_rng.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/low_level_rng.d" -MT"Application/User/low_level_rng.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/low_level_rng.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/mpu_armv8m_drv.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/mpu_armv8m_drv.d" -MT"Application/User/mpu_armv8m_drv.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/mpu_armv8m_drv.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/rsa_alt.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/rsa_alt.d" -MT"Application/User/rsa_alt.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/rsa_alt.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/sha256_alt.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/sha256_alt.d" -MT"Application/User/sha256_alt.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/sha256_alt.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/stm32l5xx_hal_msp.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/stm32l5xx_hal_msp.d" -MT"Application/User/stm32l5xx_hal_msp.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/stm32l5xx_hal_msp.o"
arm-none-eabi-gcc "../Application/User/syscalls.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/syscalls.d" -MT"Application/User/syscalls.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/syscalls.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/system_stm32l5xx.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/system_stm32l5xx.d" -MT"Application/User/system_stm32l5xx.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/system_stm32l5xx.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/tfm_bl2_shared_data.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/tfm_bl2_shared_data.d" -MT"Application/User/tfm_bl2_shared_data.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/tfm_bl2_shared_data.o"
arm-none-eabi-gcc "C:/STM32SecuWS/TFM/STM32Cube_FW_L5_V1.3.0/Projects/STM32L562E-DK/Applications/TFM/TFM_SBSFU_Boot/Src/tfm_low_level_security.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Application/User/tfm_low_level_security.d" -MT"Application/User/tfm_low_level_security.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/User/tfm_low_level_security.o"
arm-none-eabi-gcc -mcpu=cortex-m33 -c -x assembler-with-cpp -MMD -MP -MF"Application/Startup/startup_stm32l5xx_bl2.d" -MT"Application/Startup/startup_stm32l5xx_bl2.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "Application/Startup/startup_stm32l5xx_bl2.o" "../Application/Startup/startup_stm32l5xx_bl2.S"
arm-none-eabi-gcc "../image_macros_preprocessed_bl2.c" -mcpu=cortex-m33 -g3 -DSTM32L562xx -DUSE_HAL_DRIVER -DNDEBUG -DTFM_DEV_MODE '-DMCUBOOT_TARGET_CONFIG=<flash_layout.h>' '-DMBEDTLS_CONFIG_FILE=<config-boot.h>' -DMCUBOOT_DOUBLE_SIGN_VERIF -DBL2 -c -I../../Inc -I../../../../../../../Drivers/CMSIS/Include -I../../../../../../../Drivers/CMSIS/Device/ST/STM32L5xx/Include -I../../../../../../../Drivers/STM32L5xx_HAL_Driver/Inc -I../../../../../../../Middlewares/Third_Party/trustedfirmware -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/common -I../../../../../../../Middlewares/Third_Party/trustedfirmware/platform/ext/driver -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/include -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot -I../../../../../../../Middlewares/Third_Party/trustedfirmware/bl2/ext/mcuboot/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/include -I../../../../../../../Middlewares/Third_Party/mcuboot/boot/bootutil/src -I../../../../../../../Middlewares/Third_Party/mcuboot/ext/tinycrypt/lib/include -I../../../../../../../Middlewares/Third_Party/mbed-crypto/include -I../../../Linker -I../../../../../../../Drivers/BSP/STM32L562E-DK -I../../../../../../../Drivers/BSP/Components/mx25lm51245g -Os -ffunction-sections -fdata-sections -Wall -fshort-enums -fshort-wchar -funsigned-char -mcmse -Wall -Wno-format -Wno-return-type -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"image_macros_preprocessed_bl2.d" -MT"image_macros_preprocessed_bl2.o" --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -o "image_macros_preprocessed_bl2.o"
arm-none-eabi-gcc -o "TFM_SBSFU_Boot.elf" @"objects.list"   -mcpu=cortex-m33 -T"./output.ld" --specs=nosys.specs -Wl,-Map="TFM_SBSFU_Boot.map" -Wl,--gc-sections -static -Xlinker -check-sections -Xlinker -fatal-warnings --entry=Reset_Handler -Wl,--print-memory-usage,--no-wchar-size-warning -Xlinker --entry=Reset_Handler --specs=nano.specs -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
C:/ST/STM32CubeIDE_1.13.2/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.100.202509120712/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/bin/ld.exe: warning: TFM_SBSFU_Boot.elf has a LOAD segment with RWX permissions
Memory region         Used Size  Region Size  %age Used
           FLASH:       59668 B        62 KB     93.98%
     FLASH_NOHDP:        1030 B         2 KB     50.29%
             RAM:       63832 B        63 KB     98.95%
collect2.exe: error: ld returned 1 exit status
make[1]: *** [makefile:71: TFM_SBSFU_Boot.elf] Error 1
make: *** [makefile:64: all] Error 2
"make -j22 all" terminated with exit code 2. Build might be incomplete.

Seems to be a problem linking? 

So, is this a known issue? Is there another working example somewhere?

Looking at some of the documentation, it seems like ST now favours the mcuboot based SFSFU? Can this be confirmed? I had not problems compiling examples for the legacy one. 

3 REPLIES 3
loveforcircuits
Associate III

I think you have to install STM32CubeIDE 1.9 or 1.10 and build with GCC 10.x.

 

Thanks @loveforcircuits , I'm on STM32CubeIDE 2.0.0, recently updated from 1.13. Versions 1.9 and 1.10 are quite old (~4 years).

jvieira88_0-1771243493787.png

Can someone from ST side confirm that this is the case? And is there an existent project for a more recent IDE version? I wouldn't want to be using such an old IDE if not absolutely needed.

jvieira88
Associate II

Just for reference, building the example for a STM32U5 (STM32Cube_FW_U5_V1.8.0, B-U585I-IOT02A, SBSFU) works fine with a small mod to the flash_layout.h in the Linker folder where I needed to comment out the definition of MCUBOOT_PRIMARY_ONLY.