ECC key decompression in X-CUBE-CRYPTOLIB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-27 10:44 PM
I am using the X-CUBE-CRYPTOLIB (V4.2.0) in a project for STM32F207.
I am successfully able to generate ECC key pair using cmox_ecdsa_keyGen() and generate ECDSA signature using cmox_ecdsa_sign() but I am now needing to generate a shared secret using cmox_ecdh() function.
The problem I have is that the cmox_ecdh() function expects the public key in raw data format (64 bytes) but I only have the public key available in compressed format (33 bytes) where 32 bytes is the x component and the other byte indicates if the y component is odd or even. The y component can be derived from this information but I could not find a function within the X-CUBE-CRYPTOLIB that does this which means I am unable to generate the shared secret.
Is there a way of achieving this with the X-CUBE-CRYPTOLIB?
Solved! Go to Solution.
- Labels:
-
STM32CubeExpansion
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-20 7:16 AM
Hello @ncat1 ,
This compressed format is not supported for the NIST curves. so, you will need to decompress the key manually to make it suitable for use by cmox_ecdh() function.
see example in en.STM32CubeExpansion_Crypto\STM32CubeExpansion_Crypto_V4.1.0\Projects\NUCLEO-L552ZE-Q\Applications\ECC\ECDH_SharedSecretGeneration available in the Xcube_cryprolib as a reference.
the decompression can be done following this formula :
To decompress a point, we can calculate its two possible y coordinates by the formula
y1 = mod_sqrt(x3 + ax + b, p)
y2 = p - mod_sqrt(x3 + ax + b, p)
then using the odd even bit we can choose the correct one. this can be done using a python script python (see this link)
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-20 7:16 AM
Hello @ncat1 ,
This compressed format is not supported for the NIST curves. so, you will need to decompress the key manually to make it suitable for use by cmox_ecdh() function.
see example in en.STM32CubeExpansion_Crypto\STM32CubeExpansion_Crypto_V4.1.0\Projects\NUCLEO-L552ZE-Q\Applications\ECC\ECDH_SharedSecretGeneration available in the Xcube_cryprolib as a reference.
the decompression can be done following this formula :
To decompress a point, we can calculate its two possible y coordinates by the formula
y1 = mod_sqrt(x3 + ax + b, p)
y2 = p - mod_sqrt(x3 + ax + b, p)
then using the odd even bit we can choose the correct one. this can be done using a python script python (see this link)
Regards