cancel
Showing results for 
Search instead for 
Did you mean: 

Debug autentification with certificate on STM32H563

Heinz_Baumer
Associate II

Hi.

How can i connect a debug session to a device with product-state: closed and non secure software (no TZ active)

without full regression.

 

I have create the password.bin file and two certificate files with TrustZone Package Creator:

  • - DA with password
  • - DA with certificate

But i can't get a connetion to the device, neither with the password nor with the certificate file.

The message is: Wrong key file path.
But the key-file exist's and the path exists.

 

Does anyone know, how to connect?

 

 

 

 

     -------------------------------------------------------------------
                       STM32CubeProgrammer v2.18.0                  
     -------------------------------------------------------------------

Permission request submitted : 2 

Warning: Wrong key file path: D:\Projekte\ST\Product_State_Protection\password.bin 

Certificate file path submitted : D:\Projekte\ST\Product_State_Protection\DAH5_ConfigWithPassword.obk 


Start Debug Authentication Sequence

Open SDM Lib
SDMOpen                       :   624 : open       : SDM API v1.0

SDMOpen                       :   625 : open       : SDM Library version v1.2.0

open_comms                    :   513 : open       : Asserting target reset

open_comms                    :   517 : open       : Writing magic number

open_comms                    :   537 : open       : De-asserting target reset

open_comms                    :   584 : open       : Communication with the target established successfully

discovery: permission if authorized...........:(a/14) ==> Full Regression
SDMOpen                       :   624 : open       : SDM API v1.0

SDMOpen                       :   625 : open       : SDM Library version v1.2.0

open_comms                    :   513 : open       : Asserting target reset

open_comms                    :   517 : open       : Writing magic number

open_comms                    :   537 : open       : De-asserting target reset

open_comms                    :   584 : open       : Communication with the target established successfully

[00%]	discovery command
[10%]	sending discovery command
[20%]	receiving discovery
[40%]	loading credentials

 

 

 

 

 stm32cubeide_rV2jj6lTVp.jpg

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Frantz LEFRERE
ST Employee

Dear @Heinz_Baumer ,

on the STM32H563, if you do not activate Trustzone, then only password DA is possible ( certificate authentication not available).

When using the password method, only a full regression is possible.

https://www.st.com/resource/en/application_note/an6008-getting-started-with-debug-authentication-da-for-stm32-mcus-stmicroelectronics.pdf

So if you want to have the capability to reopen the debugging link, you need to activate Trustzone and use DA certificate.

Best regards,

Frantz 

View solution in original post

1 REPLY 1
Frantz LEFRERE
ST Employee

Dear @Heinz_Baumer ,

on the STM32H563, if you do not activate Trustzone, then only password DA is possible ( certificate authentication not available).

When using the password method, only a full regression is possible.

https://www.st.com/resource/en/application_note/an6008-getting-started-with-debug-authentication-da-for-stm32-mcus-stmicroelectronics.pdf

So if you want to have the capability to reopen the debugging link, you need to activate Trustzone and use DA certificate.

Best regards,

Frantz