cancel
Showing results for 
Search instead for 
Did you mean: 

CRYP_SAES_WrapKey example not working as expected: encrypted key always the same

Christian Keydel
Associate III

I am testing this with a set of STM32F573 boards, the example taken straight from CubeMX example selector for the STM32H573I-DK board without any changes. I am running it until after the call to HAL_CRYPEx_WrapKey() and before the call to HAL_CRYPEx_UnwrapKey():

  /* USER CODE BEGIN 2 */
  /* User key AESKey256 encryption*/
  if (HAL_CRYPEx_WrapKey(&hcryp, AESKey256,  Encryptedkey, TIMEOUT_VALUE) != HAL_OK)
  {
    /* Processing Error */
    Error_Handler();
  }
  /* we could not compare results, key is not known and unique for each device */

  /* User key AESKey256 decryption*/
  if (HAL_CRYPEx_UnwrapKey(&hcryp, Encryptedkey, TIMEOUT_VALUE) != HAL_OK)
  {
    /* Processing Error */
    Error_Handler();
  }

Where it says "we could not compare results, key is not known and unique for each device".

However, I am comparing results because I am expecting Encryptedkey[] to be different for each chip. But it is always the same!

When the chip has TrustZone disabled, it is (in hex):

CB3E195F 345C0D8C FAEF2E79 BD4EC0AE 78D20874 37696FBE BF1228E3 475588B5

When the chip has TrustZone enabled, it is:

FEBBE229 36B5DE56 31C1935A 28B2F8AF C2C97BE6 778413D2 EAB4AE1C F3B061A3

I've tried it with four different boards/chips, always the same result. This is clearly not working and I can't rely on the individual on-chip encryption. Please advise, thanks.

Regards,

Chris

 

1 ACCEPTED SOLUTION

Accepted Solutions
Jocelyn RICARD
ST Employee

Hello @Christian Keydel ,

What you are seeing is normal, and the example is missing one important information.

The DHUK is actually the same on all chips in OPEN state only.

As soon as you go to PROVISIONED, CLOSED, etc, the real DHUK is used and is different on each device.

If you want to check this, don't forget to provision the DA configuration. All details about that can be found in the ST wiki

Best regards

Jocelyn

View solution in original post

1 REPLY 1
Jocelyn RICARD
ST Employee

Hello @Christian Keydel ,

What you are seeing is normal, and the example is missing one important information.

The DHUK is actually the same on all chips in OPEN state only.

As soon as you go to PROVISIONED, CLOSED, etc, the real DHUK is used and is different on each device.

If you want to check this, don't forget to provision the DA configuration. All details about that can be found in the ST wiki

Best regards

Jocelyn