CRC16 CCITT/AUG bad CRC generation
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-28 11:26 AM
Hi guys,
I am testing the CRC hardware of the STM32F722ZE in the NUCLEO board, but doesn't get a right result.
The CRC keys are: Poly=0x1021 and INIT value=0x1D0F
My two data input of 16-bit wide is: [0]=0x0031 [1]=0x0032.
Some CRC calculators gives 0xEA94, but STM32 gives 0x5197
My code:
// config
CRC->INIT=0x1D0F; // init value
CRC->POL=0x1021; // Poly
CRC->CR=0x0008; // No reverses. 16-bit poly
// calculating function:
uint16_t val;
CRC->CR|=CRC_CR_RESET; // Reset
while (length>0)
{
val=*data;
CRC->DR=val;
data++;
length--;
}
What I am doing wrong ? Thak you!
And another question.. Why CRC module and DMA aren't connected directly without need interrupts ?
References - Some CRC calculators:
- Labels:
-
CRC
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-28 11:55 AM
>>What I am doing wrong ?
Try writing the data at the right width
*((volatile uint16_t *)&CRC->DR)=val;
Other than that you'd need to get more involved in the bit/byte ordering. I've posted several CRC related examples.
>>And another question.. Why CRC module and DMA aren't connected directly without need interrupts ?
Can't it just memory-to-memory via DMA2?
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-28 12:21 PM
OMG! Thank you very much! That it works!. May in the datasheet or in the AN's could notify that.
STM32F7 have buffer and stall mechanism to prevent overrun. Are you suggesting directly a DMA memory(buffer) to memory(CRC->DR) transfers without waitings?
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-28 02:32 PM
I don't recall the CRC unit having a DMA trigger source, so one could use a TIM on the same bus, or simply memory-to-memory where the destination was 16-bit (half-word) and non-incrementing.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-29 01:54 PM
Thanks mate, I will try this.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-03-30 08:08 AM
Clive, your idea is working. Thanks for your help!
This is the code for the people:
// CRC machine config:
//-----------------------------------------------------
CRC->INIT=0x1D0F; // init value
CRC->POL=0x1021; // Poy
CRC->CR=0x0008; // no reverses, 16-bit poly
// DMA2 Stream2 Channel 2 config:
//-----------------------------------------------------
DMA2_Stream2->CR&=~DMA_SxCR_EN;
DMA2_Stream2->CR=0x04002A80; // Stream2 Channel2, No burst, low priority, no double buffer, no circular, #MEM 16b no inc (CRC->DR), @PERI 16b inc(I2CBUF), MEM->MEM, DMA flow controller, no ints
DMA2_Stream2->M0AR=(uint32_t)&CRC->DR;
// No other parameters need to config. Must be configured in working function
// Working function
uint16_t crc16(uint16_t *data, uint16_t length)
{
CRC->CR|=CRC_CR_RESET; // module reset
DMA2_Stream2->PAR=(uint32_t)data; // peripheral is source
DMA2_Stream2->NDTR=length; // Num bytes transferred = 2*NDTR
DMA2->LIFCR|=0x003F0000; // Lower int flags
DMA2_Stream2->CR|=DMA_SxCR_EN; // Launch transfer
while(DMA2_Stream2->CR&DMA_SxCR_EN); // Wait while working (for testing)
return(CRC->DR & 0xFFFF);
}