cancel
Showing results for 
Search instead for 
Did you mean: 

Can i use IAR or MDK IDE programming the protection option byte (RDP) to Level 0?

lovesc1
Associate
Posted on December 17, 2014 at 02:50

In my stm32f405 level 1 is active.I can't updata mcu flash.I need change

RDP to level 0 to reprogram.

Anyone can help me?

thanks.

#stm32f4-rdp
2 REPLIES 2
Posted on December 17, 2014 at 06:24

If you have access to a serial port (USART1 or USART3) and the BOOT0 pin you could consider using the System Loader, and the Flash Loader Demonstrator.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
lovesc1
Associate
Posted on December 17, 2014 at 10:11

Thanks for you reply.

the problem has been solved.

Program code runing from internal RAM or ST-LINK utility can

solve

this problem.