2023-01-21 3:01 AM
Hello,
I've two STM32 development kit and would like to implement and test the secure boot loader, however it's not working. There is NO serial print after programming boot loader G0_BL.bin load or Application G0_App4BL.bin. I read the location of 0x08000000 and 0x08008200, i see there exists code.
The code i've referred is from the below video
Video reference: Security Part4 - STM32 security in practice - 10 Simple boot loader lab
The development kits i'm using are
Can you please help me here what i'm missing.
Thanks & Regards
Rajesh
2023-02-21 9:52 PM
2023-02-27 7:40 AM
Hello @rdund.1 ,
the new CubeU5 1.2.0 is now available here
I didn't check last week, maybe it arrived a bit late.
Best regards
Jocelyn