Win 7 to Win10 and the VCP. Oh and VB6.
Hello ST folks.
Recently, "THE MAN" updated us to Win10. Of course this broke a few (dozen) things.
Oh yes . I know VB6. Unsupported thin ice. Just like they like it around here. The story is we have a load of small TEST applications wrote with this and were quite content with them. Would LIKE to see them work as they did on Win 7. Anyway -
Win 7 :
Happily using VB and the STM32L476 and the VCP app. Modified very little from the CubeL4 Example offerings. Yes - HAL. I know. But it was quick to use.
Win 10:
Busted. As soon as I fire up a VB application that hooks to a VCP com port I get a friendly Winders banner / box. Like so-
(Imagine a box around this next couple of lines. )
RUN time error '8015' Could not set comm state., there may be one or more invalid communication parameters.
I know 8015.
No. Not Blocked with DeviceLock
No. No other device or application hogging the com port. Doesn't matter which com port I force it too I get the same result.
VCP driver tried = ST1.31, ST1.4, ST1.5, Windows INBOX driver usbser.sys. (You probably know where I got that little phrase )
Anyone else have any experience with this one?
It's somewhat of a stumper for me so far.
Thank you all !