cancel
Showing results for 
Search instead for 
Did you mean: 

Why UART IDLE Interrupt occurs after first symbol in receiving sequence?

JRaid.1
Associate

Hi!

I try to implement HAL_UART_Receive_IT + UART IDLE way to receive data, because I know maximum size of incoming messages. But i don't know size of each message anyway. To achieve this i do the following things:

1) Initialize UART and enable global UART interrupt

2) Enable UART IDLE interrupt (__HAL_UART_ENABLE_IT(&huart1, UART_IT_IDLE); )

3) Add interrupt IDLE handle into USART1_IRQHandler

void USART1_IRQHandler(void)

if (__HAL_UART_GET_FLAG(&huart1, UART_FLAG_IDLE) == SET)

{

__HAL_UART_CLEAR_IDLEFLAG(&huart1);

///...

HAL_UART_AbortReceive_IT(&huart1);

HAL_UART_Receive_IT(&huart1, (uint8_t*)bRxBuffer, 128);

}

}

///...

}

4) Initialize UART receive at main cycle

//..

HAL_UART_Receive_IT(&huart1, (uint8_t*)bRxBuffer, 128);

//..

As a result, USART IDLE occurs when first symbol recieved, but recieves sequence not finished yet.

What's it may be?

Thank you for attention in advance!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0