2023-04-27 10:57 PM
Hello,
We are using STM32F765BI series MCU. We are using SD Card using the SDIO interface. It seems that when the SDIO module is Active (CLK signal is generated at 24MHz), higher emissions are observed in the spectrum. When we disable the SDIO module (Clock stops generating 24 MHZ) then emissions are drastically reduced.
Let us know how we can eliminate the higher emissions.
Regards
Rachit Dave
2023-05-18 06:48 AM
>set all pins to SDcard to lowest possible speed. (medium or low) .
+ what speed setting you use ?
2023-05-30 11:08 PM
we have to use SD clock at 24MHz
2023-05-30 11:39 PM - edited 2023-11-20 06:53 AM
nono....the pin speed setting !
here-> medium
2023-05-31 12:01 AM
You could try surface mount ferrite bead + 1nF(?) capacitor (eg. 603 size) as the clock filter - but the higher noise could be just a symptom of other things that might need improving (eg. decoupling, ground plane design,...)