2018-09-12 05:35 PM
Hi,
I'm using 2 STM32F7-SOMs and the same program for both of them. I have ran my program on the original STM32F7-SOM, and the USB host was working. Then, I ran it on the other STM32F7-SOM, and the USB stucks at enumeration state.
Any suggestions or contributions are much appreciated.
Thank you very much.
2018-09-12 08:15 PM
Figure you'll need to debug, and scope out clocks, etc.
Check oscillators are starting, and internal clocking is working. Output internal clocks via MCO (PA8) pin. Output diagnostic/telemetry information via USART
2018-09-13 10:20 AM
Hi,
Thank you for the quick response. I'm the absolute beginner when it comes to circuit.
If you don't have time to answer all of those questions, I understand. I would be happy if you can provide me some useful links to read.
Once again.
Thank you for your time.
Have a good day.
2018-09-15 12:14 PM
Thank you. I have figured out the problem. Just the frequency issue. 48 MHZ instead of 96