Why does my UART gives a cannot access memory error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-03-10 2:13 AM
Hey everyone,
When using the default project generated my UART works fine and I can see the output on my Putty terminal. Now for my application I'm trying to move the UART object to another file.
UART.cpp:
class UART {
public:
UART();
private:
UART_HandleTypeDef huart3;
};
UART::UART(){
huart3.Instance = USART3;
huart3.Init.BaudRate = 115200;
huart3.Init.WordLength = UART_WORDLENGTH_8B;
huart3.Init.StopBits = UART_STOPBITS_1;
huart3.Init.Parity = UART_PARITY_NONE;
huart3.Init.Mode = UART_MODE_TX_RX;
huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart3.Init.OverSampling = UART_OVERSAMPLING_16;
huart3.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart3.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart3.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
HAL_UART_Init(&huart3);
HAL_UARTEx_SetTxFifoThreshold(&huart3, UART_TXFIFO_THRESHOLD_1_8);
HAL_UARTEx_SetRxFifoThreshold(&huart3, UART_RXFIFO_THRESHOLD_1_8);
HAL_UARTEx_DisableFifoMode(&huart3);
}
A function within this class sends a message using the HAL transmit function:
void UART::printMenu(){
uint8_t buff[4] = {3, 4, 5, 6};
HAL_UART_Transmit(&huart3, buff, sizeof(buff), HAL_MAX_DELAY);
char const *another = "Hello, world!\r\n";
HAL_UART_Transmit(&huart3, (uint8_t*)another, 17, HAL_MAX_DELAY);
}
Using the debugger everything is going fine, except there is nohing to be seen on the Putty terminal anymore. I think I found the issue because it can't access the memory of the buffer;
Anyone knows how to fix this issue?
Edit: probably caused by the INIT function not working as expected
/*-------------------------- USART CR1 Configuration -----------------------*/
/* Clear M, PCE, PS, TE, RE and OVER8 bits and configure
* the UART Word Length, Parity, Mode and oversampling:
* set the M bits according to huart->Init.WordLength value
* set PCE and PS bits according to huart->Init.Parity value
* set TE and RE bits according to huart->Init.Mode value
* set OVER8 bit according to huart->Init.OverSampling value */
tmpreg = (uint32_t)huart->Init.WordLength | huart->Init.Parity | huart->Init.Mode | huart->Init.OverSampling ;
MODIFY_REG(huart->Instance->CR1, USART_CR1_FIELDS, tmpreg);
While debugging I can see the CR1 is set to 12 for a fraction of a second. Only to be set to 0 again when it goes to the next line. Anyone knows why?
- Labels:
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-03-10 2:20 AM
Check that structure is cleared properly.
Looks like you have invalid data, or it subsequently gets corrupted.​
Check startup.s clearing statics and running constructors properly.​
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
‎2021-03-10 2:29 AM
I don't know how to check this. The file looks pretty advanced.
This does also look pretty strange
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-03-10 4:46 AM
I found the problem.
Seems it's better to call GPIO init AFTER the UART init haha. /facepalm