2017-04-06 3:22 AM
Hi
I am trying to use the ADC in the STM32L07 as a multichannel scan. I have set up Cube for 3 analogue channels, AN0, Temperature and VRef Int. I have set it up for single scan usign the HAL_ADC_Start_IT(&hadc); command. Within the interupt routine I am checking the ADC_FLAG_EOC for after each channel completed, and the ADC_FLAG_EOS for after the complete scan is completed. When the HAL_ADC_Start_IT is called, I see the first channel with ADC_FLAG_EOC, but straight away the ADC_FLAG_EOS is also called. I am new to the chip, and not sure what I am doing wrong, can anyone advice me? My code is below, and attached is snap shot of the cube setting
Many Thanks
Scott
unsigned ADC_Raw[3];
unsigned char ADC_index=0; #define AD_VCCINT 2 #define AD_TEMP 1void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{ if (__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOC)) { ADC_Raw[ADC_index++]=HAL_ADC_GetValue(hadc); ADC_raw = HAL_ADC_GetValue(hadc); } if (__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOS)) { <<gets called straight after first conversion... ADC_index=0; Vdd = 3000 * (*VREFINT_CAL_ADDR)/ADC_Raw[AD_VCCINT]; temperature=(((int32_t)ADC_Raw[AD_TEMP]*Vdd/3000)-(int32_t)*TEMP30_CAL_ADDR); temperature*=(int32_t)(130-30); temperature/=(int32_t)(*TEMP130_CAL_ADDR - *TEMP30_CAL_ADDR); temperature+=30; } }static void MX_ADC_Init(void)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc.Instance = ADC1; hadc.Init.OversamplingMode = DISABLE; hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc.Init.Resolution = ADC_RESOLUTION_12B; hadc.Init.SamplingTime = ADC_SAMPLETIME_1CYCLE_5; hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD; hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc.Init.ContinuousConvMode = DISABLE; hadc.Init.DiscontinuousConvMode = DISABLE; hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc.Init.DMAContinuousRequests = DISABLE; hadc.Init.EOCSelection = ADC_EOC_SINGLE_SEQ_CONV; hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc.Init.LowPowerAutoWait = DISABLE; hadc.Init.LowPowerFrequencyMode = DISABLE; hadc.Init.LowPowerAutoPowerOff = DISABLE; if (HAL_ADC_Init(&hadc) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_0; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_TEMPSENSOR; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_VREFINT; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }}
Note: this post was migrated and contained many threaded conversations, some content may be missing.2017-04-06 6:57 AM
[Speculation] When the callback gets to this bit
if (__HAL_ADC_GET_FLAG(hadc, ADC_FLAG_EOS))
the conversion sequence is all done?
2017-04-06 9:13 AM
Hi
I have placed a breakpoint at the start of the interupt, and was expected to the ADC_FLAG_EOC routine to be carried out 3 times, then on the last convertion the ADC_FLAG_EOS be done. But what I am seeing is that the ADC_FLAG_EOC is being carried out and straight away the ADC_FLAG_EOS being carried out too. I only called the HAL_ADC_Start_IT(&hadc); once so I know what I should be seeing.
I was looking at UM1749,STM32L0 HAL user manual, and it has the description below of the __HAL_ADC_GET_FLAG, but indicates it returns nothing.
Regards
Scott
__HAL_ADC_GET_FLAG Description:
Get the selected ADC's flagstatus.Parameters:__HANDLE__: ADC handle.__FLAG__: ADC flag.Return value:None2017-04-06 9:42 AM
Is the note in UM1749 for HAL_ADC_GetValue() relevant?
If sequencer is composed of 1 rank, flag EOS is equivalent to flag EOC2017-04-06 9:51 AM
hadc.Init.EOCSelection = ADC_EOC_SINGLE_SEQ_CONV;
FWIW the ADC_EOC_SINGLE_SEQ_CONV constant is marked RFU at page 99...
2017-04-06 9:59 AM
As im still learning htis chip, I assume the Rank is the position of Scan? I assume the note is only relevant if Im sampling 1 channel, but I am reading 3 in total , as below. But I notice there is only 1 rank added by Cube, in the first one. So would this cause it?
Thanks
Scott
sConfig.Channel = ADC_CHANNEL_0;
sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_TEMPSENSOR; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_VREFINT; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }2017-04-06 10:03 AM
Sorry I misread the code, the rank is the same on all channels. And I assume it indicates the channel is the rank number?
2017-04-06 10:14 AM
Thanks. I saw this, and its set to this too. I am just stuck to see what the issue can be
2017-04-06 10:48 AM
I see the define for the below is marked reserved for future use, but cubemx has the selection and created the code.
&sharpdefine ADC_EOC_SINGLE_SEQ_CONV ((uint32_t)(ADC_ISR_EOC | ADC_ISR_EOS)) /*!< reserved for future use */
2017-04-06 10:57 AM
Are any of the other channels even converting? Maybe set ranks in ascending order starting with 1 on all of your channels and for EOCSelection set that puppy to ADC_EOC_SINGLE_CONV because you want discrete ints for EOC and EOS.
As im still learning htis chipThat's cool, me too. I'm only up on the F3 and LL/std periph drivers