why can not enter TIM5 interrupt service
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-14 8:55 PM
Hello:
Today , I want to capture the high-level length of input signal using TIM5 Channel 1 (PA.0) in chip (STM32F103ZET6)?but why program can not enter TIM5 interrupt service ? please help me ! I have attached the project here #stm32f103zet6-tim5- Labels:
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-14 11:06 PM
Doesn't look unreasonable, I'd probably not be clearing interrupts immediately prior to exiting the service routine.
How are you testing the failure condition, are you breakpointing the TIM5_IRQHandler() ?Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-17 3:51 AM
Make sure that you are using startup_stmf10x_xl.s Standard lib..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-17 1:42 PM
Make sure that you are using startup_stmf10x_xl.s Standard lib..
How would that help? He has an HD part, not an XL one. And has a TIM5_IRQHandler in the vector table.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-26 3:43 AM
Yes startup_stm32f10x_hd.s lib needed. I faced the same problem while im doing Capturing using the same board. By default it will add the (startup_stm32f10x_md.s) lib. In startup_stm32f10x_md.s lib there is no TIM5, so startup_stm32f10x_hd.s file has to be added..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-08-26 9:57 AM
I faced the same problem while im doing Capturing using the same board.
What board is that? The OP doesn't identify one, and it's not the STM32 VL-Discovery board. He also attaches a project that contains the right source files, and right defines for the HD part. From the project one might infer he has a Core103Z.By default it will add the (startup_stm32f10x_md.s) lib. What does? The template project, for the STM3210E-EVAL doesn't, or the VL-DISCOVERY. I can see that using the wrong file, with a vector table lacking the interrupt required, will be a problem. I'm just not seeing that in the project presented here. There is some other issue at play here. The OP has not responded.Up vote any posts that you find helpful, it shows what's working..