2014-07-18 1:37 AM
I keep getting stuck in an infinite loop in this function
while(!__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_FLAG_RXOVERR | SDIO_FLAG_DCRCFAIL | SDIO_FLAG_DTIMEOUT | SDIO_FLAG_DBCKEND | SDIO_FLAG_STBITERR)) and I am able to look up what the flags mean, but I was wondering if there is an easy way to tell which one is causing the problem. Also, I am using keil v5, c++, and stm32 eval board. Thanks. #eval #c++ #keil2014-07-18 1:59 AM
Hi Phillîp,
Using the debugger, try to look into SDIO status register content (SDIO_STA). Definition of this register bits is in the reference manual (RM0090). -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2014-07-18 3:43 AM
It seems like all of the bits in that register are 0