2018-02-13 01:40 AM
I am Kapil Sharma,
I have custom Board.When i am trying to debug code running successfully and the Command log of Keil shows this..
* JLink Info: Found SW-DP with ID 0x2BA01477
* JLink Info: Found SW-DP with ID 0x2BA01477* JLink Info: Scanning AP map to find all available APs* JLink Info: AP[1]: Stopped AP scan as end of AP map has been reached* JLink Info: AP[0]: AHB-AP (IDR: 0x24770011)* JLink Info: Iterating through AP map to find AHB-AP to use* JLink Info: AP[0]: Core found* JLink Info: AP[0]: AHB-AP ROM base: 0xE00FF000* JLink Info: CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)* JLink Info: Found Cortex-M4 r0p1, Little endian.* JLink Info: FPUnit: 6 code (BP) slots and 2 literal slots* JLink Info: CoreSight components:* JLink Info: ROMTbl[0] @ E00FF000* JLink Info: ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7* JLink Info: ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT* JLink Info: ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB* JLink Info: ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM* JLink Info: ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU* JLink Info: ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETMROMTableAddr = 0xE00FF000* JLink Info: Reset: Halt core after reset via DEMCR.VC_CORERESET.* JLink Info: Reset: Reset device via AIRCR.SYSRESETREQ.can you provide me any solution for my problem?
2018-02-13 02:00 AM
What problem ?
I can't see any error message in the log.
And the question is 'assumed answered' anyway ...
2018-02-13 02:05 AM
While i am debugging the code the comment log shows below
* JLink Info: Reset: Halt core after reset via DEMCR.VC_CORERESET.
* JLink Info: Reset: Reset device via AIRCR.SYSRESETREQ.2018-02-13 04:21 AM
And how do you come to think of this as an error ?
The debug adapter resets the core in order to invoke the reset vector/handler, and start the user application.