cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 CubeMX 4.23.0 bug (ADC1+DMA+TIM6_TRGO)

leshich-k
Associate II
Posted on November 08, 2017 at 12:33

Generated a project for STM32F746 (Firmware Package for Family STM32F7 v1.8.0) that uses ADC1 + DMA + TIM6 (TRGO) for Keil MDA-ARM 5. Tried to run it - no trigger is received by ADC, so no convertion data is transferred over DMA.

The bug is documented in 'STM32F74xxx STM32F75xxx Errata sheet', page 7 (2.2.1). Workaround is to turn on CLOCK for DAC.

Please fix the bug in code generating .

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on November 08, 2017 at 15:51

Hello,

I raised this issue internally to the CubeMx team for further check and investigation.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Jeanne Joly
Senior III
Posted on February 13, 2018 at 14:22

Hi

Kozyrev.Alexey

,

It should be available in the next CubeMX release.

I will keep you informed.

BR. Jeanne