cancel
Showing results for 
Search instead for 
Did you mean: 

Which version of matlab can use the MAT-TARGET models for simulink? really working for 2015b?

vguil
Associate

Hello,

I have matlab 2015b and I can not use simulink blocks of MAT-TARGET whereas the datasheet v2.2 claims that it can.

Simulink tells me that the blocks have been done with a newer version (R2016b) and can not be used.

Is there older blocks for 2015b?

Regards

2 REPLIES 2
S.Ma
Principal

The databrief should be updated with supported version of matlab.

Besides this, 2015 was Windows VISTA era, quite a while ago too.

As an embedded project would last 1-2 years, going 4 years in the past seems a bit long.

Cyril FENARD
ST Employee

​Hi @vguil​ ,

The version 5.1.0 of STM32-MAT/TARGET has just been released at the end of July 2019.

Document RN0087 has also been updated accordingly.

Regards.

Cyril