2018-10-20 05:36 PM
Floating Point in Hardware, is it M3 and above ? L series ?
Which processors have Double Floating Point in Hardware ?
F7, H7 ?
2018-10-20 05:49 PM
F3 F4 F7 are Single Precision FP in hardware
F76x F77x and H7xx have the new DPFPU
2018-10-20 05:49 PM
F3 F4 F7 are Single Precision FP in hardware
F76x F77x and H7xx have the new DPFPU
L151 is based on M3 but has no FP in hardware
2018-10-20 06:48 PM
The STM32L443 has the hardware SPFP but less timers.
The new STM32L4R series has 16+ timers. and DSI.
2018-10-21 12:29 AM
Floating point is available in all devices based on Cortex-M4, M7 or M33 cores.
Double floating point is available on some F7 and H7.