cancel
Showing results for 
Search instead for 
Did you mean: 

Which MCUs are suitable for PLC?

VKaki
Associate

We are looking for design programmable logic controller. Please recommend us which microcontroller suits our application

3 REPLIES 3

You've explained your application requirements exceedingly poorly.​ Very few here are interested in doing your due diligence work.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
VKaki
Associate

Specifications:

UARTs - 4

SPI - 2

I2C - 2

CAN

Ethernet

SD Card

ADC - 8 - 12bit

NAND Flash

SRAM

Operating Frequency: 120MHz to 400MHz

We are expecting system in such a way that the User can build their application program using ladder logic or any other standard PLC programming languages.

Our system should operate based on user applications

Please share us which of the MCU /MPU is best suitable for our application.

Amel NASRI
ST Employee

Hi @VKaki​ ,

First recommendation is to use the MCU finder (from ST web site, as embedded on STM32CubeMX tool or as standalone tool) to look for MCUs that meet your requirement.

Please note that ST supplies some PLC solutions. You can refer to this page on ST web site for more details.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.