2021-01-11 10:37 PM
We are looking for design programmable logic controller. Please recommend us which microcontroller suits our application
2021-01-11 11:18 PM
You've explained your application requirements exceedingly poorly. Very few here are interested in doing your due diligence work.
2021-01-12 12:55 AM
Specifications:
UARTs - 4
SPI - 2
I2C - 2
CAN
Ethernet
SD Card
ADC - 8 - 12bit
NAND Flash
SRAM
Operating Frequency: 120MHz to 400MHz
We are expecting system in such a way that the User can build their application program using ladder logic or any other standard PLC programming languages.
Our system should operate based on user applications
Please share us which of the MCU /MPU is best suitable for our application.
2021-01-15 02:27 AM
Hi @VKaki ,
First recommendation is to use the MCU finder (from ST web site, as embedded on STM32CubeMX tool or as standalone tool) to look for MCUs that meet your requirement.
Please note that ST supplies some PLC solutions. You can refer to this page on ST web site for more details.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.