2022-07-27 6:55 AM
hi,
this is the first time i have used QSPI library, I have to use external flash in QSPI mode.
In the data sheet it is given that, CS# pin should be low until command instruction 16bit data will pass. as shown ablove.
but when executing command the CS# Pin perform HIGH-LOW_HIGH and again did the same thing at the timing of writing. this should not happen. asper data it low at command insertion and data writing.
ihave check ON CRO.
my question where is the CS# micro, so that i can manage to write.
i know this could be stupid question.
thanking you.
if (HAL_QSPI_Command(&QSPIHandle, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return QSPI_ERROR;
}
Solved! Go to Solution.
2022-07-30 5:56 AM
For enabling the QSPI mode, you need to set QEN bit of configuration bit and for that you have to send write enable command followed by 16 bit value of status register and configuration register. In that sequence CS# should be low.
given in data sheet. i have attached screen shotbut when I write code for enabling command given below
int32_t QSPI_EnterQPIMode(QSPI_HandleTypeDef *Ctx)
{
QSPI_CommandTypeDef s_command;
uint8_t reg_data[] = {0x02, 0x02};
/* Enable write operations */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = 0x01; /* equal on both memory types */
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_NONE;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&QSPIHandle, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return QSPI_ERROR;
}
if (HAL_QSPI_Transmit(&QSPIHandle, reg_data, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return QSPI_ERROR;
}
return QSPI_OK;
}
the CS# pin get two time HIGH_LOW sequence, where in datasheet(screen shot above) it should be done in consecutive.
CS# pin screen shot for enterQPI mode.i think because of this i am not getting proper result, so if I manipulate CS pin, result would be proper. correct if am wrong .
thanking you
2022-07-27 11:20 AM
It's controlled properly/directly by the Peripheral, and via the AF setting of the associated pin.
The data sheet would list those pins usable for this.
The CS would be held low for Data transfer if you've got some DataMode and NbBytes set in the device instance (QSPIHandle), and you subsequently issue a HAL_QSPI_Receive()
Note that you can have a more open-ended/protracted transaction using the HAL_QSPI_AutoPolling() function, which waits for specific conditions in the read data to be met, and then dumps the CS
There's probably a section in the Reference Manual on this..
2022-07-30 2:36 AM
i have search all the code, but i dint see any CS# low micro.
and there is no such thing in reference manual.
please provide if you got this.
thanking you.
2022-07-30 5:19 AM
The questions lose something in translation
Some aspects controlled in configuration
hQspi->Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE; /* Min 50ns required after non Read command */
hQspi->Init.ClockMode = QSPI_CLOCK_MODE_0;
hQspi->Init.FlashID = QSPI_FLASH_ID_1; /* Default value at start, can be changed dynamically using BSP_QSPI_SetFlashID() */
The peripheral owns the pin control
/* QSPI BK1 CS GPIO pin configuration */
gpio_init_structure.Pin = QSPI_BK1_CS_PIN;
gpio_init_structure.Pull = GPIO_PULLUP;
gpio_init_structure.Alternate = QSPI_BK1_CS_PIN_AF;
HAL_GPIO_Init(QSPI_BK1_CS_GPIO_PORT, &gpio_init_structure);
These setting use by HAL_QSPI_Command and HAL_QSPI_Receive/Transmit ultimately determine how the peripheral holds the NCS signal. Normal behaviour is NCS drops at the beginning of the command dispatch, and then raises it at the end of the data transaction.
s_command.AddressSize = QSPI_ADDRESS_32_BITS;
s_command.AlternateBytes = 4;
s_command.DummyCycles = 8;
s_command.NbData = Size;
It is not a GPIO you can control manually, it is driven by the peripheral's state-machine, based on settings/parameters configured.
2022-07-30 5:29 AM
NCS Low spans multiple phases, or subset as necessary, per command structure
NCS LOW
CMD + ADDR + ALTERNATE + DUMMY + DATA
NCS HIGH
Polling looks something like
NCS LOW
CMD + [DATA, REPEAT UNTIL MATCH]
NCS HIGH
In timeout case transaction needs to be aborted in some cases, to release NCS
2022-07-30 5:56 AM
For enabling the QSPI mode, you need to set QEN bit of configuration bit and for that you have to send write enable command followed by 16 bit value of status register and configuration register. In that sequence CS# should be low.
given in data sheet. i have attached screen shotbut when I write code for enabling command given below
int32_t QSPI_EnterQPIMode(QSPI_HandleTypeDef *Ctx)
{
QSPI_CommandTypeDef s_command;
uint8_t reg_data[] = {0x02, 0x02};
/* Enable write operations */
s_command.InstructionMode = QSPI_INSTRUCTION_1_LINE;
s_command.Instruction = 0x01; /* equal on both memory types */
s_command.AddressMode = QSPI_ADDRESS_NONE;
s_command.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = QSPI_DATA_NONE;
s_command.DummyCycles = 0;
s_command.NbData = 2;
s_command.DdrMode = QSPI_DDR_MODE_DISABLE;
s_command.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
s_command.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
if (HAL_QSPI_Command(&QSPIHandle, &s_command, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return QSPI_ERROR;
}
if (HAL_QSPI_Transmit(&QSPIHandle, reg_data, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return QSPI_ERROR;
}
return QSPI_OK;
}
the CS# pin get two time HIGH_LOW sequence, where in datasheet(screen shot above) it should be done in consecutive.
CS# pin screen shot for enterQPI mode.i think because of this i am not getting proper result, so if I manipulate CS pin, result would be proper. correct if am wrong .
thanking you
2022-07-30 6:55 AM
The screen shot of the scope lacks any contextual data. Really need clock+data
To write the registers you'll be needing at least two commands, so two NCS pulses.
Presumably a Write Enable, followed by a Write Register(s), and potentially a Polling for BUSY in situations where the write goes to NV or OTP which operates more slowly than combinatorial logic.
Also you might want to read the current register settings, only setting the bits of interest, and when necessary, rather than blind writing.