cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I download Demo code for STM32F769-DISC0? Is it possible to program the board in ubuntu 18.04? If it is, then please provide the tutorials or guidance urls.

TGUDL
Associate II

Recently we bought the STM32F769-Disc0 development board. We want the source code of demo project and how to compile the code in ubuntu 18.04 or any versions of ubuntu.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Bernie
Associate II

Mahesh,

I've developed an open-source codebase which has disco-based demo code, Ubuntu 18.04-based, gcc, CMake. Detailed installation instructions. I'm soliciting feedback for it. Only difference in your case, however, is that I used a STM34F407 Disco board. Should be close.

https://bitbucket.org/burnwood/raging-release/src/default/

Bernie

Demos can usually be found in the Cube/HAL example trees

STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I-Discovery\Demonstrations\STemWin\Binary\STM32769I-DISCO_DEMO_V1.0.0_FULL.hex

Can be flashed with tools like STM32 Cube Programmer application

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..