2017-08-06 03:58 PM
STM have made a big song and dance about STM32H7 devices being in production by Q2 2017. Well Q2 has come and gone and still distributors such as Digi-Key and Mouser have no inventory nor even any parts listings. Also when is STM going to make available discovery boards for this series?
#stm32h72017-08-07 04:26 PM
Dear @David,
See this Thread
https://community.st.com/0D50X00009XkdsFSAR
. If you need a board please contact your nearest ST sales office.Cheers
STOne-
2017-08-08 05:10 AM
Do you really mean to approach Digikey, Mouser or Farnell?
2017-08-08 01:17 PM
Hi David,
Sure it is coming and also our lowest cost Nucleo boards. It is just a matter of time when we finish the product qualification using our cutting edge 40nm eFlash node and fixing some erratas. Stay tuned. { Do not ask me when ? ...I will escape the question... }
Cheers
STOne -32
2017-08-08 03:09 PM
What I am also asking is, will STM be providing a lower cost STM32H743-DISCO discovery board? I see ST's web site has a STM32H743I-EVAL high end evaluation board listed but these evaluation boards are generally very expensive for the non-professional. and usually offer far more than is really needed to get started.
Also the STM32H743I-EVAL board is not available yet from any distributor. So when will development hardware of any kind be available at (North American) distributors?And while I have STM's attention, why oh why, are you still insisting on only 2 x 32 bit timers but 10 x 16 bit timers. I've just downloaded the STM32H743xI datasheet and almost fell off my chair laughing at the fact that this super high performance 32 bit ARM microcontroller still has only 2 x 32 bit timers. Why is STM so stubborn with not providing more true 32 bit timers on a chip like this at the top end of your range? Come on now, it's about high time you changed that!!!2017-08-08 04:04 PM
...and completely ignore the timer question.
2017-08-08 04:25 PM
No, he means the ST sales office for your local region. The ones they have dotted around Europe, UK and USA, etc.
Pounding on the local distributor might help, or sales reps who carry ST on their line card.
2017-08-08 04:45 PM
Hi David H, David L ,
Regarding 32-bit Timer question. It is a smart one, However most if our cutomers and users wanted a product with easy user experience to migrate from an STM32F4 to STM32H7 as example and 16-bit timers are a MUST for legacy code. Take an exemple of FOC algo for White goods 32-bits Timers are exotic !
Innovation is a matter of small steps nowadays to meet market acceptance and mass adaption. Take exemple of Smartphones for the last decade, Simple functions of few mechanical buttons still there for power on / off, volume increase / decrease.
Cheers
STOne -32.
2017-08-08 05:11 PM
Hi STOne-32,
The 40nm eFlash of the H7 will also be used in lower-end, low cost, microcontrollers (with less SRAM, Flash and CPU clock) or this technology is only economic viable for high-end application processor kind microcontrollers?
In others words,
Ari.
2017-08-08 05:25 PM
Hi mendes,
At the moment for high-end MCUs > 200MHz Clock. But from technology point of view it is also good for low end MCUs and will be the future trend after today 180nm/90nm to reduce wafer cost so end price for our customers.
Cheers.
STOne-32.