2017-05-01 06:57 AM
E.g the F767 offers 4 dfu interfaces:
.. alt=3, name='@Device Feature/0xFFFF0000/01*004 e', serial='395734643435'
... alt=2, name='@OTP Memory /0x1FF0F000/01*001Ke,01*032 e', serial='395734643435'... alt=1, name='@Option Bytes /0x1FFF0000/01*032 e', serial='395734643435'... alt=0, name='@Internal Flash /0x08000000/04*032Kg,01*128Kg,07*256Kg', serial='395734643435While I understand alternate interface 0-2, I don't find any information about the 'Device feature interface' . An3156 Table 6. mentions it as introduced with V2.1, but gives no further hint.
2017-05-05 02:22 AM
Nobody has an idea?
2017-05-08 05:08 AM
Hi,
You may refer to the
(page 29) for more clarification.Thanks
Imen
2017-05-08 07:56 AM
Thnaks for the answer.
However the phrase 'device feature set' is no mentioned in section 3.4 'Bootloader Memory management' . I proposed to add the phrase 'device feature set' somehow in that section.