cancel
Showing results for 
Search instead for 
Did you mean: 

What's the correct power consumption on STM32F413

paker earth
Associate II
Posted on March 09, 2017 at 15:50

Hi all:

The document says the power consumption is 112 uA / MHz.

But the power supply has offered 56mA current.

I measure the  IDD pin, the result is only 16 mA.

Is the consumption due to  ST-Link part ?

If yes, could I cut off the ST-Link part?

Thank you in advance. 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
S.Ma
Principal
Posted on March 09, 2017 at 16:07

The datasheet contains multiple power consumption scenario. Find the entry which is closest to your situation (supply, MHz, peripheral on or off, etc..) What is on a datasheet is guaranteed and more specific. (let's say second order of precision). I haven't looked at the schematic to understand where the current is going after the jumper... check it out.