2018-02-20 3:12 PM
Hello, I am currently using an STM32F301K6U. STM32CubeMX allows me to set pretty much any GPIO as a 'GPIOP_Analog'. However, when I go into the ADC1 under 'Peripherals' every single item is red because there is some conflict with another pin. The ST Micro rep told me I could set any GPIO as an analog input or output, so I am not understanding how this is supposed to work. How do I do an analog read on the GPIO I set as 'GPIO_Analog'? And similarly, do an analog out on these pins as well?
Thanks and any help/advice is greatly appreciated.
2018-02-20 3:24 PM
The data sheet breaks down those connected to an ADC, ie ADC123_IN4
The reason to turn ANY pin to analogue is to turn OFF the schmitt trigger on the input that feeds down stream digital logic and GPIOx->IDR, etc. This avoids noise, and potential oscillation.
Use the ADC to measure the supported pins, use the DAC to output to supported pins. Review the Data Sheet
2018-02-20 5:26 PM
Thank you
Turvey.Clive.002
for this answer. On the top of what you said I would like to add that switching off GPIO's Schmitt trigger also decreases a bit current consumption of MCU. That is why Analog Input is a recommended mode for all GPIOs, which are unused by application.Analog Input is a default mode of GPIOs inlow-power STM32 MCUs: STM32L0 and STM32L4. For other STM32 familiesuser has to take care about configuring unused GPIOs in Analog Input mode. This task can be easily done with STM32CubeMX:
Regards
Szymon
2018-02-20 5:28 PM
Thank you for this info. Yeah I went over the datasheet before creating the PCB and this was not very clear to me. Do you mind mentioning which page you are referring to and possible a small explanation? The datasheet in regards to ADC and DAC is very confusing.
2018-02-20 5:37 PM
PA0 Channel1 of ADC1
PA1
Channel2 of ADC1PA2
Channel3 of ADC1PA3
Channel4 of ADC1PA4 Channel5 of ADC1 or Channel 1 of DAC1