How can I generate a roughly 3 ms pulse on PG14 (=non-timer pin) when SystemCoreClock is 216 MHz?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-20 3:41 AM
I am working with the STM32F769 microcontroller (SystemCoreClock: 216 MHz) and I need to generate a roughly 3 ms pulse (negative pulse is also ok), that is always exactly the same, on pin PG14 for calibration purposes. According to STM32CubeMX, the pin can be configured as the following:
ETH_TXD1
FMC_A25
LPTIM1_ETR
LTDC_B0
QUADSPI_BK2_IO3
SPI6_MOSI
SYS_TRACED1
USART6_TX
GPIO_Input
GPIO_Output
GPIO_Analog
EVENTOUT
GPIO_EXTI14
The only thing I can think of is to use the USART6_TX, but to make it run so slow I'd have to temporarily slow down the APB2 Prescalar. The microcontroller is running FreeRTOS with TIM6 as the TICK-clock and TIM6 is located on APB1 so I guess this solution is acceptable, but I would really prefer something where I don't have to fiddle with the clock settings. Can anybody please recommend something better?
- Labels:
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-20 4:11 AM
Never mind, I realize I made a mistake, it works fine to clock the USART at 3333 Baud and with a word length of 9 bits I end up with a 3 ms negative pulse if I transmit 0b000000000. If an administrator sees this, please feel free to delete this thread.