2018-06-28 1:53 PM
hello .
1.We have done a Stm32F429 board , and we can set PDR ON to GND OR VCC (we set to gnd)
how ever in the STM32 PDF : AN4488 Application note STM32F4xxxx MCU hardware
it says in IN ....3.2.1 PDR_ON
PDR_ON = 0 is mostly intended for VDD supply between 1.7 V and 1.9V (i.e. 1.8V +/- 5% supply). Supply ranges which never go below 1.8V minimum should be better managed with internal circuitry (no additional component thanks to fully embedded reset controller). • To ensure safe power down, the external voltage supervisor (or equivalent) is required to drive PDR_ON=1 during power off sequence
1.1 we done PDR ON CONNECT to GND we use 3.3V -3.0 V to the mcu did we set pdr_on correct ?
when should i use pdr_on to vcc and when to gnd please explain in more practical example .
thanks
yaniv
2018-06-28 3:03 PM
Hello,
as explained in application note you are referring to, in case you need any of features below, PDR_ON must be tied to VCC:
When the internal reset is OFF, the following integrated features are no longer supported:
• The integrated power-on reset (POR) / power-down reset (PDR) circuitry is disabled.
• The brownout reset (BOR) circuitry must be disabled.
• The embedded programmable voltage detector (PVD) is disabled.
• VBAT functionality is no more available and VBAT pin should be connected to VDD.
2018-06-29 12:29 AM
thanks for your answare ,
1. still not 100% cear '
in case you need any of features below' do you mean below 1.8V meaning power source is 1.7V ?
2,we use use vdd as 3.3V so PDR_ON should be tied to vss (gnd)
thanks
yaniv
2018-06-29 4:42 PM
Dear Gentleman,
if your VDD is 3.3V PDR_ON pin MUST be connected to VDD. It is dangerous to connect to GND , in case of voltage drop ; the MCU can not work properly after next power up. There is a special sequence to be followed at startup as explained in AN4488.
in your case of
mailto:VDD@3.3V
you must connect to VDD.Cheers,
STOne-32 .