cancel
Showing results for 
Search instead for 
Did you mean: 

What is the "debug" column in the MAP file?

Chris Rice
Associate III

I know this is a dumb question, but I've googled it and can't get an explanation. What is the "debug" column in the MAP file?

Also, it's alarmingly big... using Keil is there a setting I should use to compile without whatever is taking up that space? I don't see the typical debug/release config settings.

Thanks for the help.

==============================================================================
 
 
      Code (inc. data)   RO Data    RW Data    ZI Data      Debug   
 
    206256      18706     599208       7644     443828    3533745   Grand Totals
    206256      18706     599208       1628     443828    3533745   ELF Image Totals (compressed)
    206256      18706     599208       1628          0          0   ROM Totals

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

It's stuff allowing the debugger e.g. to relate memory positions to variables, program counter to lines in the source etc.

Don't be alarmed, it's doesn't occupy a single bit on the mcu, it's all on the PC in the .elf file.

JW

View solution in original post

3 REPLIES 3
waclawek.jan
Super User

It's stuff allowing the debugger e.g. to relate memory positions to variables, program counter to lines in the source etc.

Don't be alarmed, it's doesn't occupy a single bit on the mcu, it's all on the PC in the .elf file.

JW

There is a "Debug Information" check box in the Output options pane.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Chris Rice
Associate III

Thank you!