cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H573: Ethernet

jowakar122
Associate III

I am using STM32H573 and trying to enable ethernet. I have used the below article for it:
https://community.st.com/t5/stm32-mcus/how-to-use-the-lwip-ethernet-middleware-on-the-stm32h5-series/ta-p/691100

But ethernet is not being initialized. The HAL_ETH_Init is returning error which is resulting in error handler.

jowakar122_0-1747656677963.png

This is the condition being checked in MX_ETH_Init function. As even after using the steps mentioned in the article mentioned above the ethernet is not working. 
- Do we have to add RX and TX descriptors specific addresses in the linker file?

0 REPLIES 0