cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum STM32F7 TIM1 PWM frequency?

choies1
Associate
Posted on March 22, 2018 at 16:02

Now I am using STM32F7 Discovery board. I want to make TIM1 PWM with high frequency.

I made 10MHz PWM frequency. However, I can't increase the PWM frequency even though I change '

Prescaler

 ' and 'Period '

.

htim1.Init.Prescaler = n;

htim1.Init.Period = m;

As I know I can make PWM frequency to System Frequency(216MHz) using TIM1.

If possible, please let me know the setting code.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on March 22, 2018 at 16:36

The TIM clocks at 216 MHz, but your period and pulse are going to be multiple of 4.6ns, so I'd assume frequencies of less than 108 MHz, and clearly not interrupting more than 1/100th of that.

Ceiling shouldn't be hard to demonstrate.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
henry.dick
Senior II
Posted on March 22, 2018 at 17:12

'What is the maximum STM32F7 TIM1 PWM frequency?'

depending on what you are asking.

the timer can run with a period of 1 -> output frequency of 216Mhz / 2.

however, whether your GPIO can run at that frequency is a separate question;

whether you can do anything useful with that kind of frequency / resolution is another;

whether it makes sense for you to run PWM at that kind of frequency still another. I would say that unless you know what you are doing, needing PWM over 1Mhz means you are doing something seriously wrong.