cancel
Showing results for 
Search instead for 
Did you mean: 

What is the efficient way to measure the time taken by ADC DMA conversion?

BSale.1
Associate II

I toggle a GPIO pin in the ADC call back function, I get time values on the oscilloscope close what is the supposed to be according to the datasheet, is that correct and efficient? Is there a method better maybe?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

Set up continuous conversions, monitor the pin on an oscilloscope directly at the pin or as close as practical and you should be able to see the effect when the sampling capacitor is connected or disconnected. Measure the distance between events on the scope.

If you feel a post has answered your question, please click "Accept as Solution".

That is what I did, I got values close to 3 to 3.2uS which is close to the calculate value from the datasheet which is 2.9uS.