cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between pins FDCAN1_TX and FDCAN1_TXFD_MODE ?

Mr_M_from_G
Senior II

Hello ,

in STM32 H742 data sheet I find CAN pind with or without the suffix FD_MODE, but there is no explanation on it. What does that mean? CAN peripheral has only one output for Rx and Tx each. Can't I use those without FD_MODE when using CANFD but only for CAN2.0? How does the pin know which mode is used?

Thank you for some details

Martin

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
3 REPLIES 3
Mr_M_from_G
Senior II

Any ideas?

I need this information for a schematics, which pins should I use?

Thanks for any help

Martin

Mr_M_from_G
Senior II
mƎALLEm
ST Employee

Dear @Mr_M_from_G​ ,

Indeed, only Rx and Tx are used for FDCAN communication..

All FDCANx_TXFD_MODE & FDCANx_RXFD_MODE occurrences will be removed from datasheets.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.