cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between FDCAN1 and FDCAN2?

wsuwa.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KDJEM.1
ST Employee

Hello @wsuwa.1​ ,

Which STM32 product you are using?

If you used STM32H750, the TTCAN protocol level 1 and level 2 is supported only for FDCAN1. This protocol is not supported for FDCAN2.

For more explanation, you can refer to RM0433 and precisely section 56.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.