cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between a STM32l071K series vs STM32l)72K series

Harish gopal R
Associate
Posted on May 30, 2017 at 14:45

Actually we are working on the communication between a LoRa module(sx1272) and an STM32l071kxx microcontroller through an spi interface. We got some source code for STM32l072Kxx series so we need to know the actual difference between these two will help us out ......

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on May 30, 2017 at 15:44

Hi

harish

,

You can refer to the datasheet of used product

http://www.st.com/content/ccc/resource/technical/document/datasheet/b5/24/80/11/51/59/47/f7/DM00141pdf/files/DM00141pdf/jcr:content/translations/en.DM00141pdf

and

http://www.st.com/content/ccc/resource/technical/document/datasheet/98/e1/71/c0/ae/f5/4b/d4/DM00141pdf/files/DM00141pdf/jcr:content/translations/en.DM00141pdf

.

The datasheet

should be the reference for comparisons

of used product.

Thanks

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Uwe Bonnes
Principal III
Posted on May 30, 2017 at 16:22

Main differences are missing USB, TSC, DAC and RNG on L071.