2021-07-12 12:34 AM
i read data sheet of lis2dh and lis3mdl. i am using st linux driver to read raw data of accelerometer and magnetometer. Now when i set sampling frequency 1600 for accelerometer i get data of x axis at 40 ms. when i set sampling frequency 80 for magnetometer i get data of x axis at 60 ms.
Actually i want to get that data at highest speed.
as per datasheet when odr of accelerometer is 1600 hz then data need to come at 0.0625 ms and when odr of magnetometer is 80 hz then data need to come at 12.5 msec.
why i am not getting data at 0.625 ms and 12.5 ms from magnetometer and accelerometer ?
where is my mistake ?