2019-02-28 2:19 AM
Hello All,
I am using a NUCLEO-F401RE Board and a IKS01A2 Sensor Board with it. I want to collect the incoming data dynamically and modify it.
By using Unicleo-GUI and just clicking Connect and Start I am able to observe the collected data. I want to collect this same data through the serial COM port by running a Python Script which replicates only these 'Connect' and 'Start' clicks.
Please can someone tell me which commands I should send in order to get data from the NUCLEO board.
Thanks.
2020-03-07 11:55 AM
Hello @engtec ,
I am trying to implement a similar application but for the sensortile box. I was wondering if you were able to figure out a way to use python in order to extract the data through the serial port.
Any help or guidance would be much appreciated.
Thanks,
VRao.1