2022-02-03 10:15 PM
I have a PCA design which I'd like to support both devices with min configuration changes in the PCB dependent on the fitted device. I've made provision VACP1/2 options - either CAP or 0R resistor to VSS.
2022-02-04 06:50 AM
You can get a reasonable answer from this using CubeMX.
They are quite different chips. Unlikely for the code to be compatible even if the footprint can be managed.