2024-03-25 2:56 AM
Hi,
I'm using STM32U575I-EV and CubeMX.
Please tell me about benefits using lpbam in CubeMX.
I thought that if I properly set up the peripherals that support LPBAM on the "Pinout & Configuration" screen, I could do the same thing as LPBAM Scenario.
When is it better to use LPBAM Scenario ?
Best regards.
2024-03-25 3:10 AM
Hello @DK3
Two major advantages result from using LPBAM subsystem mechanisms:
Bus and kernel clocks are distributed only when needed.
Most of the product parts can be shut down.
Analog peripherals or oscillators are powered on only when necessary.
Peripheral configurations are done by DMA instead of CPU.
Data transfers are done by DMA instead of CPU.
For more details, I suggest you refer to this WIKI and the AN5645.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.