2021-09-21 1:23 PM
STM32F405 using STLIBF4 v1.4.0
Near the beginning of my code, I enable the windowed watchdog with
WWDG_Enable()Shortly thereafter, I have a conditional block that executes only if the windowed watchdog is enabled, i.e.
if ((WWDG->CR & WWDG_CR_WDGA) != 0)
{
// do stuff
}If this condition is checked immediately after the WWDG_Enable() call, the block fails to execute. However, if I move this conditional block later in the code (ensuring that some time has passed after enabling the watchdog), the block will execute as expected.
Through in-circuit debugging, I have confirmed that the WDGA bit in the WWDG_CR register does not read as set immediately after the execution of WWDG_Enable().
Please help me understand this behavior. Is the value of the WWDG_CR register only updated on the edge of PCLK1?
2021-09-24 12:54 PM
Not discussed in any great detail, but RM0090, 2.1.11 AHB/APB bridges (APB):
[...] Before using a peripheral you have to enable its clock in the
RCC_AHBxENR or RCC_APBxENR register.
JW
2021-09-24 3:14 PM
Great. Thank you for your patience. That should be enough information for me develop a solution.