cancel
Showing results for 
Search instead for 
Did you mean: 

CCID USBD transfer block on F1

Ayoub-Marghoub
Associate II

Split from this thread 


My firmware is based on this ccid usbd driver https://github.com/STMicroelectronics/stm32-mw-usb-device/blob/master/Class/CCID/Src/usbd_ccid.c .

The issue that I face, the PC finishes receiving data immediately after receiving 256 bytes (10 bytes of header + 246 bytes of data). when I want to send to pc 253 bytes of data + 10 bytes of header (263 bytes in total) by splitting (64 bytes by 64 bytes) the PC finishes receiving data immediately after receiving the fourth chunk which is 256 bytes (10 bytes of header and 243 bytes of data), It doesn't wait for the fifth chunk, which carries the remaining 7 bytes of my data which arrives in an unknown message despite the fact that I define the size of the data to be sent as 253 bytes. Images 1 and 2 show these details captured by wireshark software.1122

this is my code used to send data by chunks :

uint8_t SC_Itf_XferBlock(uint8_t *ptrBlock, uint32_t blockLen, uint16_t expectedLen,
                         USBD_CCID_BulkIn_DataTypeDef *CCID_BulkIn_Data)
{
  uint8_t ErrorCode = SLOT_NO_ERROR;
  UNUSED(CCID_BulkIn_Data);
  UNUSED(expectedLen);
  UNUSED(blockLen);
  UNUSED(ptrBlock);

  if (ProtocolNUM_OUT == 0x00U)
  {
    /* Add your code here */
  }

  if (ProtocolNUM_OUT == 0x01U)
  {
    /* Add your code here */


  data_to_send_size = 253;
  

  CCID_BulkIn_Data->dwLength = data_to_send_size;
  memcpy(CCID_BulkIn_Data->abData, data_to_send, data_to_send_size);

  if (data_to_send_size > 54U)
  {
      tx_remaining_ptr = &data_to_send[54];
      tx_remaining_len = data_to_send_size - 54;
      tx_in_progress   = 1;
  }
  else
  {
      tx_remaining_ptr = NULL;
      tx_remaining_len = 0;
      tx_in_progress   = 0;
  }

  }

  if (ErrorCode != SLOT_NO_ERROR)
  {
    return ErrorCode;
  }

  return ErrorCode;
}
static uint8_t USBD_CCID_DataIn(USBD_HandleTypeDef *pdev, uint8_t epnum)
{
  USBD_CCID_HandleTypeDef *hccid = (USBD_CCID_HandleTypeDef *)pdev->pClassDataCmsit[pdev->classId];

#ifdef USE_USBD_COMPOSITE
  /* Get the Endpoints addresses allocated for this class instance */
  CCIDInEpAdd  = USBD_CoreGetEPAdd(pdev, USBD_EP_IN, USBD_EP_TYPE_BULK, (uint8_t)pdev->classId);
  CCIDCmdEpAdd = USBD_CoreGetEPAdd(pdev, USBD_EP_IN, USBD_EP_TYPE_INTR, (uint8_t)pdev->classId);
#endif /* USE_USBD_COMPOSITE */

  if (epnum == (CCIDInEpAdd & 0x7FU))
  {
    /* Filter the epnum by masking with 0x7f (mask of IN Direction)  */

    /*************** Handle Bulk Transfer IN data completion  *****************/

    switch (hccid->blkt_state)
    {
      case CCID_STATE_SEND_RESP:

        /* won't wait ack to avoid missing a command */
    if(tx_in_progress && tx_remaining_len > 0)
    {
    uint8_t chunk = (tx_remaining_len > 64) ? 64 : tx_remaining_len;

    USBD_LL_Transmit(pdev, CCIDInEpAdd, (uint8_t *)tx_remaining_ptr, chunk);

    tx_remaining_ptr += chunk;
    tx_remaining_len -= chunk;
    }
    else
    {
    tx_in_progress = 0;

hccid->blkt_state = CCID_STATE_IDLE;

/* Prepare EP to Receive  Cmd */
(void)USBD_LL_PrepareReceive(pdev, CCID_OUT_EP,
hccid->data, hccid->MaxPcktLen);
    }

        break;

      default:
        break;
    }
  }
  else if (epnum == (CCIDCmdEpAdd & 0x7FU))
  {
    /* Filter the epnum by masking with 0x7f (mask of IN Direction)  */

    /*************** Handle Interrupt Transfer IN data completion  *****************/

    (void)USBD_CCID_IntMessage(pdev);
  }
  else
  {
    return (uint8_t)USBD_FAIL;
  }

  return (uint8_t)USBD_OK;
}



1 ACCEPTED SOLUTION

Accepted Solutions
4 REPLIES 4
FBL
ST Employee

HI  @Ayoub-Marghoub 

Your custom modification in USBD_CCID_DataIn is not recommended.

In my understanding, CCID is length driven, not chunk driven. I mean, the host does not wait for a fifth chunk just because you intended one. It should wait for:

  • the number of bytes declared in the CCID header
  • or a short packet that terminates the transfer

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

resolved

Ayoub-Marghoub
Associate II

I resolved this issue, thanks.

FBL
ST Employee

Hi @Ayoub-Marghoub 

 

 

Could you please share how you resolved the issue, so it can help other community members as well?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL