2018-09-30 11:22 PM
Hello!
I bought a NUKLEO-F767ZI. I want to program a virtual COM port in CubeMX and Keil uVision5, but device's manager in my WINDOWS10 says "The Windows system stopped this device because it reported a problem." (Code 43) The request for the descriptor failed USB devices. "
But the built-in ST-LINK/V2-1 works well.
I tried many methods to fix this error, but nothing helps me.
Tell me please, where i can find Samples and Exaples for NUKLEO-F767ZI to program VCP?
Thanks!
2018-10-01 4:55 AM
The should be assorted examples under the CubeF7 code trees, unpack and review. CubeMX should have unpacked in the repository.
2018-10-01 2:42 PM
Thank you!
Tell me please, which folder is the repository?
2018-10-01 4:49 PM
It depends where you unpacked it!
Search for something like:
STM32Cube_FW_F7_V1.12.0
and then see the Projects under that and find the most applicable directory.
James