Question
vetor table symbol Not found?
Posted on July 27, 2016 at 12:02
I can't debug anymore, I get this message after copying the interrupt table to RAM, even if I comment the Remap() funtion I get this error. Even if I load and try to debug another project I get this error. I seems Once I Execute this once I get this faulty operating device. Wed Jul 27, 2016 12:01:19: Warning: __vector_table symbol not found. e_entry value: 0x0800514C does not match reset vector value: 0x0800513C Initial SP_main value:0x20000E08 uncertain. Wed Jul 27, 2016 12:01:19: Target reset Wed Jul 27, 2016 12:01:20: One or more breakpoints could not be set and have been disabled.