cancel
Showing results for 
Search instead for 
Did you mean: 

VCAP layout

MikeDB
Lead

I'm sure everyone else has noticed how the two pins to VCAP seem to be placed just over a complete side of the package away so there is bound to be some resistance/inductance in the tracking. I was wondering if anybody has ever hit problems with this, or how thick the tracking should be. Also the datasheets and app notes seem a bit inconsistent, some say 2.2uF, some two 2.2uF in parallel and others 4.7uF. Prefer to get the board right first time. Processor is a STMH7 series in 100 pin QFP

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
waclawek.jan
Super User

You are not supposed to connect those two VCAP pins with a track, and you are supposed to place a 2.2uF cap on each.

Get inspired with the Nucleo, I know it's a 144-pin package but the principle is the same.

JW

View solution in original post

2 REPLIES 2
waclawek.jan
Super User

You are not supposed to connect those two VCAP pins with a track, and you are supposed to place a 2.2uF cap on each.

Get inspired with the Nucleo, I know it's a 144-pin package but the principle is the same.

JW

Ah that makes more sense. Thanks