2014-02-21 1:37 PM
Hi,
I'working with USB to send data from my F3 Discovery to the PC. For that i used the CDC class. I managed to send few bytes of data using the routine below:
uint8_t TabInt[6]={80,90,88,99,10,13};uint8_t *ptr_int=TabInt;
uint16_t Lentgh_int=sizeof(TabInt);
CDC_Send_DATA(ptr_int, sizeof(Lentgh_int));
/*--------- CDC Definition-------------*/
uint32_t CDC_Send_DATA (uint8_t *ptrBuffer, uint8_t Send_length)
{
/*if max buffer is Not reached*/
if(Send_length < VIRTUAL_COM_PORT_DATA_SIZE)
{
/*Sent flag*/
packet_sent = 0;
/* send packet to PMA*/
UserToPMABufferCopy((unsigned char*)ptrBuffer, ENDP1_TXADDR, Send_length);
SetEPTxCount(ENDP1, Send_length);
SetEPTxValid(ENDP1);
}
else
{
return 0;
}
return 1;}As we can see the data to be sent is declared as u8. It Tried to do the same for the data but with no success.
float_t TabKs[2]={1.215,1.245}; uint8_t *ptr_Ks=(uint8_t*)&TabKs; uint8_t Lentgh_Ks=sizeof(TabKs);CDC_Send_DATA(ptr_Ks, Lentgh_Ks);
Unfortunately that didn't work for me,The problem i think is that my float value is being sent as one byte and i have to reconstitute it correctly but i don'k know how. If you have an idea how can i resolve my issue, i would be grateful.
Thanks in advance.
2014-02-22 12:25 PM
I resolved the problem. It was in the C# interface that i made for that purpose.
2014-03-01 12:54 AM
Hi, i already have this board and i'm trying to communicate with my pc by cdc (to send gyroscope angle, i posted a [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/Newbie%20on%20stm32%20%28USB%20HID%20or%20CDC%20on%20f3%20discovery%29&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx¤tviews=8]message about it on this forum). I 'm newbie on stm and your code can interrest me to progress and understand the logic. It's possible that you send me your code (specialy for cdc communication ...) ?
Thanks in advance2014-03-04 1:23 PM