cancel
Showing results for 
Search instead for 
Did you mean: 

Using STM32H562ZI with I3C v1.0 compatible I3C Target endpoint

srinathkp
Associate II

Hi,

I'm planning to use STM32H562ZI as I3C controller with an I3C v1.0 compatible Target endpoint. Since STM32 I3C IP supports I3C v1.1.1, will there be any potential issues on RSTDAA, ENTDAA, I3C Private Write, I3C Private Read or other electrical parameters with v1.0 ? Though I do not see any limitation based on v1.0 & v1.1.1 specifications (Apart from IBI mandatory byte and new CCCs), I'd like to hear from the community. Appreciate the help.

Thanks,
Srinath

1 ACCEPTED SOLUTION

Accepted Solutions
srinathkp
Associate II

ST team reached out directly and STM32H562ZI is backward compatible with I3C v1.0.

This can be marked as resolved now.


View solution in original post

2 REPLIES 2
Billy OWEN
ST Employee

Hi @srinathkp 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy

srinathkp
Associate II

ST team reached out directly and STM32H562ZI is backward compatible with I3C v1.0.

This can be marked as resolved now.