Using RTC Wake up ISR as OS Systick
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-04-05 12:48 PM
Due to low power requirements, I would like to use a different source to generate the 1ms or 10ms OS tick. The internal RTC, using a 32768Hz external crystal as it's clock source, is able to generate interrupts at ~61us increments if the wake up ISR is setup to auto interrupt periodically. In our STM32L152xD device, I was able to setup the interrupt and see that it jumps to the ISR, but it seems it is happening a lot faster that expected based on the Asynchronous/Synchronous pre-scaler registers. What values would I need to write to these registers to get a 1ms interrupt? I programmed them with 2, and 10 to give (2+1)*(10+1) = 33, then 32768/33 = ~993 Hz. I declared a unsigned long variable which is incremented each time interrupt takes place, but the values I read after placing a break point in the code are in the millions! Not even possible in the lowest interval of 63us. The WUTF bit in the RTC->ISR register is cleared in the ISR as the first line of code.
Any suggestions? Thanks Galan #stm32l152-rtc-configuration- Labels:
-
STM32L1 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-04-15 8:25 AM
Hi goharlaee.mano.002,
As mentioned in the application notehttp://www.st.com/web/en/resource/technical/document/application_note/DM00025071.pdf
''Using the hardware real time clock (RTC)'' : The minimum wakeup period that you can get is 122,07 us. But there is no need for RTC in your case ! To use clock other than SysTick to generate the tick interrupt you ought to generate ab interrupt from a timer other than Systick:Provide an implementation of vPortSetupTimerInterrupt() that generates an interrupt at the frequency specified by the configTICK_RATE_HZ FreeRTOSConfig.h constant.
Install xPortSysTickHandler() as the handler for the timer interrupt, and ensure xPortSysTickHandler() is not mapped to SysTick_Handler() in FreeRTOSConfig.h, or renamed as SysTick_Handler() in port.c.
This is mentioned in the
http://www.st.com/st-web-ui/static/active/jp/resource/technical/document/user_manual/DM00105262.pdf
: “Developing Applications on STM32Cube With RTOS� Another information , if you need to use other HAL time base than Systick and keep Systick as only FreeRtos Timer base ( to prevent dead lock issue) you ought to select a timer as HAL time base source. Refer to ''HAL_TimeBase'' example inhttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243
at this path: STM32Cube_FW_F4_V1.11.0\Projects\STM32469I_EVAL\Examples\HAL\HAL_TimeBase (You can do that using platform, in SYS table -> Timerbase Source )-Hannibal-